Create Automated Tests Using BenchVue Test Flow

BenchVue Test Flow is an embedded application which runs within the BenchVue desktop. You can use the BenchVue Test Flow to quickly create and analyze automated tests – without any programming. With the intuitive drag-and-drop interface, Test Flow allows you to combine multiple instruments into an automated test for better characterization of your device-under-test. The specific controls and properties supported by Test Flow will vary depending on the instrument type and model number.

Make sure you have installed the main BenchVue application prior to using the Test Flow feature.

To enable the Test Flow, click "BenchVue Test Flow" switch. If main BenchVue application is not already running, the main BenchVue application will launch automatically in a separate window. Launch the BenchVue Test Flow application from the main BenchVue application.

To create a Sequence using Test Flow, use your mouse to drag the desired blocks (outlined with orange rectangles) from the Oscilloscope application and drop them into the Sequence Workspace on the BenchVue Test Flow application.


For more information on using the Test Flow, see the Help file for the BenchVue Test Flow application as shown below.